Question
Hello, I am working on STC3117 for voltage and SoC detection. So far I am able to get voltage correctly but current values and SoC are wrong. Please check configuration if anything wrong.
Configurations are as follow
I am using default OCV table and 660mAh battery (4.2v max) with <70 mOhm internal impedance
first OCV value = 7788
REG_CTRL
vBattTWI_Write(1, BATT_GAUGE_ADD, REG_CTRL, 0x02);
REG_MODE
vBattTWI_Write(1, BATT_GAUGE_ADD, REG_MODE, 0x30);
After configure current value
current = 65533
and
OCV = 7103
Final values while monitor I am getting
I = -1 mA
SoC = 80%
Charge value = 52
#STC3117