Skip to main content
SJain.3
Visitor II
May 24, 2021
Question

H2PAK-2 vs H2PAK-6 MOSFET package for high current application

  • May 24, 2021
  • 1 reply
  • 2450 views

I'm using multiple MOSFET of STH310N10F7 in parallel for current of approximately 60A.

MOSFET are used in DC Bias and not switching so time delay is not a factor of consideration.

I'm confused between the packages.

What are intended application of H2PAK-2 vs H2PAK-6 package? Which is suggested for pure DC bias application?

    This topic has been closed for replies.

    1 reply

    Peter BENSCH
    ST Technical Moderator
    May 25, 2021

    H2PAK-2 is fully compatible with the D2PAK footprint, making it easy to upgrade.

    H2PAK-6 offers some advantages in passing the low Rdson to the board.

    The chip inside and parameters are identical, so both can be used for the same application.

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.