Skip to main content
HIbra.1
Visitor II
Oct 31, 2022 8:29 AM UTC
Question

Greetings all, I am working with the gate driver STDRIVE101 to drive a BLDC motor. For the current sensing opamps, the value of the filter capacitor was calculated based on the cut-off frequency, my question is, does this cutoff frequency depend on F

Fsw is the switching frequency of the Mosfets, i am asking if this value should be considered when calculating the filter capacitor value or not

This topic has been closed for replies.

2 replies

Cristiana SCARAMEL
ST Employee
Nov 3, 2022 3:11 PM UTC

Hello @HIbra.1​ and welcome to the ST Community.

Are you using our EVALSTDRIVE101 demonstration board or a custom board?

In the second case, could you share the schematic?

To set the cut-off filter frequency you have to consider two points:

  • the target is to filter ringing on PWM rising edges
  • the filtering effect slows down the PWM edge (therefore waiting more time to sample)

You must find a tradeoff between these aspects.

In general a cut-off frequency of the order of 1 MHz can be enough.

Moreover take into account that the OpAmp has its own limited bandwidth that acts as filter itself

(e.g. GBWP = 10 MHz, setting a gain of 10 --> BW = 1 MHz).

I hope this post can help you; if so, consider to mark it as best answer by clicking the label "Select as Best".

"If you feel a post has answered your question, please click ""Accept as Solution"""
Cristiana SCARAMEL
ST Employee
Nov 24, 2022 8:41 AM UTC

Hello @HIbra.1​ there are updates from you?

"If you feel a post has answered your question, please click ""Accept as Solution"""