Skip to main content
d_hug
Associate
December 1, 2015
Question

getting started with the l6384e

  • December 1, 2015
  • 2 replies
  • 848 views
Posted on December 01, 2015 at 19:37

Hello,

I set up the following minimal circuit to get started with the l6384e high voltage half-bridge driver[1]:

0690X00000605dCQAQ.png

Vcc is 5V. And with the 100K resistor on DT/SD I measure 2.2V. Which is well above the Vdt=0.5V as given in table 5 of [1], hence the device should be enabled.

Now following the timing diagram in figure 3 in the datasheet[1], I would expect LVG to be high. Unfortunately it is 0V.

Is my expectation wrong? Did I miss something?

Thank you.

[1]: http://www.st.com/web/en/resource/technical/document/datasheet/CD00169715.pdf

#l6384
This topic has been closed for replies.

2 replies

d_hug
d_hugAuthor
Associate
December 4, 2015
Posted on December 04, 2015 at 12:16

I thought I checked for Vcc requirements. I should have rechecked before posting here.

The solution is that the l6384e has undervoltage lockout and in table 7 of [1]:

Parameter                      Typ.

--------------------------     ----

VCC UV turn-on threshold        12V

VCC UV turn-off threshold       10V

Sorry for that.

[1]: http://www.st.com/web/en/resource/technical/document/datasheet/CD00169715.pdf
Pedro Oliveira
Associate II
June 7, 2017
Posted on June 07, 2017 at 21:17

Hi, i'm having the same kind of problem with the L6384E. I'm using 12V on the Vcc, do you think it should works?

The strange thing about my aplication is the Vce, the voltage on Collector e Emissor doesn't get steady. As shown on the image.

0690X00000607GKQAY.png