Skip to main content
TPate.2
Associate
Sep 1, 2021 1:38 PM UTC
Solved

Getting Started with STEVAL - SPIN3202.

Hello, I got board STEVAL - SPIN3202 and i want to use it with BLDC motor. how i will get getting started with it? i even not found any example. can anyone direct me to that? Thanks.

This topic has been closed for replies.
Bruno_STBest answer
ST Employee
Sep 1, 2021 3:03 PM UTC

Hello @TPate.2​ ,

You can start by downloading the X-CUBE-MCSDK, then select launch application under MC_SDK_5.4.7\Utilities\PC_Software\STMCWB\STMCWB.exe, then click on new project Application if any, NewProject->SelectBoards = Inverter then Control = STEVAL-SPIN3202.

After this Generation, will generate some code for you with the desired IDE.

If you want more details about program and tool, you can find some documentation under MC_SDK_5.4.7\Documentation, especially UM2374.

BR,

Bruno

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

7 replies

Bruno_STBest answer
ST Employee
Sep 1, 2021 3:03 PM UTC

Hello @TPate.2​ ,

You can start by downloading the X-CUBE-MCSDK, then select launch application under MC_SDK_5.4.7\Utilities\PC_Software\STMCWB\STMCWB.exe, then click on new project Application if any, NewProject->SelectBoards = Inverter then Control = STEVAL-SPIN3202.

After this Generation, will generate some code for you with the desired IDE.

If you want more details about program and tool, you can find some documentation under MC_SDK_5.4.7\Documentation, especially UM2374.

BR,

Bruno

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
TPate.2
TPate.2Author
Associate
Sep 2, 2021 5:17 AM UTC

i followed steps of STMCWB. but when i am going to connect serial port in Motor Monitor 3.6 in UM2374. it shows "Connection failed! No response. Check communication cable, the power on the board or the baudrate." also i saw code while(1) in main() is empty. was i made any mistake or i need to write code there?

ST Employee
Sep 2, 2021 7:52 AM UTC

@TPate.2​  please make sure you select appropriate port and baud rate to 9600 baud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ST Employee
Sep 2, 2021 7:53 AM UTC

Yes, main code is empty, UART and MC tasks executed under systick()

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Cristiana SCARAMEL
ST Employee
Sep 2, 2021 7:13 AM UTC

Hi @TPate.2​ ,

for more details on STEVAL-SPIN3202 board configuration you can refer to the "Documentation Tab" in the product page:

  • UM2278: Getting started with the STEVAL-SPIN3202 evaluation board, advanced BLDC controller with embedded STM32 MCU
  • UM2168: Using STM32 motor control workbench with STSPIN32F0 and STSPIN32F0A

Let me know if these info help you.

"If you feel a post has answered your question, please click ""Accept as Solution"""
KToth.1
Associate
Sep 29, 2021 5:57 AM UTC

hi,

make sure to connect the power supply too, beside the usb cable