Skip to main content
easchlut
Associate
July 17, 2003
Question

generate an Interrupt, when the motor don't turn

  • July 17, 2003
  • 2 replies
  • 673 views
Posted on July 17, 2003 at 10:38

generate an Interrupt, when the motor don't turn

This topic has been closed for replies.

2 replies

maxime2399
Associate III
May 17, 2011
Posted on May 17, 2011 at 10:16

Your problem seems difficult... I have never done it myself, this is just a short analysis of the question.

The way the internal state machine is done, it is impossible to have the Z event (BEMF zero crossing) unless you had before the commutation C and the demagnetization D.

- The commutation: you can imagine having a commutation and a very low voltage/current applied

- The demagnetisation: this should not be a problem, a software demagnetisation is a just a dead time for the BEMF.

The second problem I see is linked to your high side swithes. You have to be careful if you use a bootstrap power supply for the drivers.

The drivers will stop working if you stop commuting the low side switches.

The other approach is just by pooling the comparator output.
easchlut
easchlutAuthor
Associate
May 17, 2011
Posted on May 17, 2011 at 10:16

Hello

I have a problem I need the ST72141 as a generator. I want to regulate the speed if the motor is externally propelled. For this I need the zerocrossing times which passed in the Interrupt. But I don't have Interrupts in this mode. In the normal mode when the motor is driven by the processor althing is okay.

Have anyone an idea?

Thanks

Kicker