For the L6235Q: What is the maximum PWM frequency for the FWD/REV pin or EN pin if I wish to use them for motor control?
I would like to use a PWM to control motor speed in our particular design (like what is described in DT0001), but I could not find in the datasheet where a maximum PWM frequency, minimum high time, and minimum low time are specified for EN or FWD/REV. What is the maximum PWM frequency to the FWD/REV pin on the L6235Q for using a PWM to drive speed and direction per DT0001? For EN, it seems it must be longer than TD(off)EN + TD(on)EN times...