Question
For POWERSTEP01 : while using STEPCLK/DIR mode as well as internal motion engine mode I would like to know
- Is there any speed limit or acceleration enforced in step/dir mode? 60min/s*1.67MHz/200st/128uSt = 3260RPM max speed theoretical. What about acceleration in this case?
- What is the thermal resistance junction to air with minimal copper footprint?
- What is the thermal resistance junction to air with 2oz 1in^2 copper plane?
- What is the reverse recovery time of the body diode in the internal H bridges of the POWERSTEP01?
- How will the output slew rate change as a function of Vs? It is specified in Table 11 for 48V, can you give the equivalent data for 30V and 36V?
- Are the dissipation levels for internal regulators typical values, or worst case? What are the conditions for these numbers?
- Under what conditions can the device operate at 10Arms of coil current? At 48V, I would estimate that is approximately 10W of dissipation in the device. Is that accurate?