Skip to main content
BTrem.1
Senior
May 24, 2020
Question

Example program needed to setup and use the STM32 pid_regulator?

  • May 24, 2020
  • 0 replies
  • 423 views

I'd like to see a simple example program that allows the user to setup the pid_regulator in the STM32 motor code. I'm using the FOC library and want to add an external loop around the speed control to do phase correction. The STM32 code is good at obfuscating all useful information.

This topic has been closed for replies.