As a rule, the internal bootstrap circuit for supplying the high-side FET is sufficient and advantageous because the external diode with all its disadvantages can be saved.
However, there are cases where an external diode is useful - the AN1299 describes some of these in section 1. Don't be confused by the description L638xE tricks and tipps, at that time the L6498 did not yet exist, but the principle is the same.
Good luck!
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
/Peter
In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.