Skip to main content
walterma
Associate III
April 10, 2009
Question

ERROR on Hall handled by TIM4

  • April 10, 2009
  • 3 replies
  • 692 views
Posted on April 10, 2009 at 10:53

ERROR on Hall handled by TIM4

This topic has been closed for replies.

3 replies

walterma
waltermaAuthor
Associate III
May 17, 2011
Posted on May 17, 2011 at 10:15

Hi Billino,

thank you, I found also that error at the GPIO initialization.

There are also a few errors at the definitions of some constants. For example you can find in MC_pwm_3shunt_prm.h following:

#define PHASE_A_ADC_CHANNEL ADC_Channel_11

#define PHASE_A_GPIO_PORT GPIOC

#define PHASE_A_GPIO_PIN GPIO_Pin_1

#define PHASE_B_ADC_CHANNEL ADC_Channel_12

#define PHASE_B_GPIO_PORT GPIOC

#define PHASE_B_GPIO_PIN GPIO_Pin_2

#define PHASE_C_ADC_CHANNEL ADC_Channel_13

#define PHASE_C_GPIO_PORT GPIOC

#define PHASE_C_GPIO_PIN GPIO_Pin_3

but in the c-file you don't use this constants:

/* ADC1, ADC2, PWM pins configurations -------------------------------------*/

GPIO_StructInit(&GPIO_InitStructure);

/****** Configure PC.00,01,2,3,4 (ADC Channels [10..14]) as analog input ****/

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_3 |GPIO_Pin_4;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AIN;

GPIO_Init(GPIOC, &GPIO_InitStructure);

and you define the same constants in the c-file (stm32f10x_svpwm_3shunt.c):

#define PHASE_A_ADC_CHANNEL ADC_Channel_11

#define PHASE_B_ADC_CHANNEL ADC_Channel_12

#define PHASE_C_ADC_CHANNEL ADC_Channel_13

that's not very useful :)

I build a brushless controller with the STM32F103C8T6 and I use TIM4 for the hall-sensors, TIM1 (not remapped) for the PWMs and ADC_Channel_0, ADC_Channel_1, ADC_Channel_2 for zero-crossing-detection. I know that using constants for pin-declarations is hard, because the ports can also change and so on.. Please use the constants in your c-files instead of hard-coding.

regards

Walter Craffonara

stello
Visitor II
May 17, 2011
Posted on May 17, 2011 at 10:15

Hello Walterma,

thanks for your bug reporting. Unfortunately I also have to say you should pay attention at GPIO initialization where

#else // TIMER4_HANDLES_HALL

/* TIM4 clock source enable */

RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM4, ENABLE);

/* Enable GPIOB, clock */

RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB, ENABLE);

/* Configure PB.06,07,08 as Hall sensors input */

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6, GPIO_Pin_7, GPIO_Pin_8;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;

GPIO_Init(GPIOB, &GPIO_InitStructure);

#endif

should be

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6|GPIO_Pin_7| GPIO_Pin_8;

Regards,

Billino

walterma
waltermaAuthor
Associate III
May 17, 2011
Posted on May 17, 2011 at 10:15

Hi,

I want to report an error in the file stm32f10x_hall.c :

If you use the TIM4 to handle the Hall sensors, the function ReadHallState(void) should be as follows:

u8 ReadHallState(void)

{

u8 ReadValue;

#if defined(TIMER2_HANDLES_HALL)

ReadValue = (u8)(GPIO_ReadInputData(GPIOA)) & GPIO_MSK;

#elif defined(TIMER3_HANDLES_HALL)

ReadValue = GPIO_ReadInputDataBit(GPIOB, GPIO_Pin_0)<

ReadValue |= GPIO_ReadInputDataBit(GPIOA, GPIO_Pin_6)<

ReadValue |= GPIO_ReadInputDataBit(GPIOA, GPIO_Pin_7);

#elif defined(TIMER4_HANDLES_HALL)

ReadValue = ((u8)(GPIO_ReadInputData(GPIOB))>>6) & GPIO_MSK;

#endif

return(ReadValue);

}

instead of

u8 ReadHallState(void)

{

u8 ReadValue;

#if defined(TIMER2_HANDLES_HALL)

ReadValue = (u8)(GPIO_ReadInputData(GPIOA)) & GPIO_MSK;

#elif defined(TIMER3_HANDLES_HALL)

ReadValue = GPIO_ReadInputDataBit(GPIOB, GPIO_Pin_0)<

ReadValue |= GPIO_ReadInputDataBit(GPIOA, GPIO_Pin_6)<

ReadValue |= GPIO_ReadInputDataBit(GPIOA, GPIO_Pin_7);

#elif defined(TIMER4_HANDLES_HALL)

ReadValue = ((u8)(GPIO_ReadInputData(GPIOA))>>6) & GPIO_MSK;

#endif

return(ReadValue);

}

The error is that you read the input data from the wrong port!

[ This message was edited by: walterma on 06-04-2009 17:03 ]