Skip to main content
Visitor II
July 18, 2024
Question

dynamic resistance of TVS

Dear Sirs,

Could you advise me dynamic resistance(Rd) of TVS such as SM6T33CAY used to clamp against pulse 5B per ISO 7637-2 or load dump B in ISO 16750-2.load dump B_1.JPG 

Its voltage source waveform is clamped instead of exponential surge curve.

Thanks

John 

This topic has been closed for replies.

1 reply

Peter BENSCH
ST Technical Moderator
July 29, 2024

Welcome @JMan, to the community!

The question should be answered as you have already connected with your local contact so this thread can be closed?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.