Skip to main content
Associate
November 27, 2024
Solved

droput voltage for LDL1117

I just bought 10 pcs of LDL1117S33R which i plan to use them to power 3.3V modules form a 4V regulated source.

According to the data sheet the typical dropout is 350mV and max is 600mV @1.2A. My module consumes less than 500mA, so i expect to have enough margin with a Vin of 4V to get 3.3V at the ouput. But the module doesnt boot at 4V input.

When measured the dropuout is 1V -  1.1V. Did anybody face this problem?

The chips are labeled LL33 F329 with ST logo

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
November 27, 2024

@ves011 The max 600mV for the LDL1117 is specified for an input voltage that is at least 1V above the output voltage. With your small voltage difference, I would recommend switching to an ultra-low dropout LDO, e.g. the LD39100PU33R.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

11 replies

Andrew Neil
Super User
November 27, 2024

@ves011 wrote:

My module consumes less than 500mA


How is that determined? Is that the average operating current?

 


@ves011 wrote:

But the module doesn't boot at 4V input.


Often the current required to boot is more - sometimes much more - than the operating current ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
mƎALLEm
ST Technical Moderator
November 27, 2024

@Andrew Neil wrote:


Often the current required to boot is more - sometimes much more - than the operating current ...


Called "inrush current" : 

https://www.matsusada.com/support/terms/ps/rush-current.html

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Andrew Neil
Super User
November 27, 2024

Show your schematic

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
November 27, 2024

@ves011 The max 600mV for the LDL1117 is specified for an input voltage that is at least 1V above the output voltage. With your small voltage difference, I would recommend switching to an ultra-low dropout LDO, e.g. the LD39100PU33R.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ves011Author
Associate
November 27, 2024

@Peter BENSCH 

Yep! RFM :)

Will look into LD39100PU33R