Skip to main content
florian
Associate
March 19, 2014
Question

driving STEVAL-IHM023V2 without controller

  • March 19, 2014
  • 12 replies
  • 1542 views
Posted on March 19, 2014 at 17:24

We are working with the STEVAL-IHM023V2 to drive a brushless DC motor of 24V. The set up is to be used in an academic environment and will be used as set up for students. As it is their task to make the control algorithm (from current set point to switching pattern based on Hall sensors) we did not buy the controller of ST. The tests we did so far were successful but it is not possible to keep one leg of the inverter open (in a stable way). The only way we found so far to keep both upper and lower switch open was to keep both connection points floating (which cannot be the right option). Is there anyone who has tried to do the same and knows a solution?

#steval-ihm023v2
This topic has been closed for replies.

12 replies

florian
florianAuthor
Associate
April 1, 2014
Posted on April 01, 2014 at 15:25

Hello Gigi,

that could be an explanation for the problem... But if you ask me, that should be a paragraph of text in the datasheet ;) By the end of the week I will test the board on the motor.

Thank you for your help and I'll let you know if everything works fine.

Kind regards,

Florian

florian
florianAuthor
Associate
April 3, 2014
Posted on April 03, 2014 at 08:29

The motor is turning around smoothly :)