Skip to main content
FKamm.2
Associate
April 26, 2022
Question

Does a switching regulator effect the output of a buck converter with a fixed output voltage of +5 V like the L7805?

I'm trying to design an voltage regulator on a motor control board. I want an output voltage of 5 VDC and the input voltage is 24 VDC. Because of heat production i was thinking about using a switching regulator like the L7983 followed by an L7805. But I'm unsure if the frequency of the switching regulator will effect the output signal of the L7805. I need the 5V for the microcontroller and the current sense amplifier.

Or is there an easier way?

Thank you very much

    This topic has been closed for replies.

    14 replies

    Harvey White
    Senior III
    May 7, 2022

    There's a replacement for the 7805 regulator, which is a 3 pin switching regulator to which you can add a filter. Check with Digikey, who seems to stock them. They're about 2-3 USD each, and can tolerate a higher input voltage. Haven't use them in a design yet.