Skip to main content
JTorr.7
Visitor II
May 9, 2023
Question

Did the L298HN ever have leads that were the same 5.28mm length ? The data sheet only shows one option where lead L6 is 2.38mm, and the other lead L5 is 5.28.

..

This topic has been closed for replies.

1 reply

Peter BENSCH
ST Technical Moderator
May 10, 2023

Welcome, @JTorr.7​, to the community!

I have checked it again: the L298HN has had exactly this pin configuration since at least the year 2000, i.e. the inner pins are 2.38mm from the bottom edge of the device, the outer pins 5.28mm.

Does it help?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.