Skip to main content
MS123
Visitor II
January 12, 2019
Question

Cooling of L6201PS Motor Driver

  • January 12, 2019
  • 0 replies
  • 477 views

I want to use the L6201PS Motor Driver for a motor (24-48V) and the max. current is 4A. My Question is at which current value do I need a coolant? I found out in the datasheet that I only need some ground area for cooling, is that correct?

This topic has been closed for replies.