Skip to main content
val_ltd
Associate III
May 14, 2015
Question

Configuring SPI HAL driver to control L6482H

  • May 14, 2015
  • 1 reply
  • 590 views
Posted on May 14, 2015 at 07:49

Hello,

I need a right SPI configuration and Send_Receive_byte() funtion for using with STM32F4, STM32CubeMX 4.7.0 and HAL drivers... Does anyone have it?

I have a project running fine with STM32F4xx StdPeriph_Driver V1.2.0 to connect my STM32F4 and my L6482H chips.

Now, I am trying to migrate my code, for using STM32 CubeMX v4.7.0 and HAL drivers. See below:

void

HAL_SPI_MspInit

(SPI_HandleTypeDef* hspi)

{

  GPIO_InitTypeDef GPIO_InitStruct;

  if(hspi->Instance==SPI1)

  {

    /* Peripheral clock enable */

    __SPI1_CLK_ENABLE();

 

    /**SPI1 GPIO Configuration    

    PA5     ------> SPI1_SCK

    PA6     ------> SPI1_MISO

    PA7     ------> SPI1_MOSI

*/

    GPIO_InitStruct.Pin = GPIO_PIN_5|GPIO_PIN_6|GPIO_PIN_7;

    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

    GPIO_InitStruct.Pull = GPIO_NOPULL;

    GPIO_InitStruct.Speed = GPIO_SPEED_FAST;

    GPIO_InitStruct.Alternate = GPIO_AF5_SPI1;

    HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

  /* System interrupt init*/

    HAL_NVIC_SetPriority(SPI1_IRQn, 1, 0);

    HAL_NVIC_EnableIRQ(SPI1_IRQn);

  }

}

----------------------------------------------------------

/* SPI1 init function */

void

MX_SPI1_Init

(void)

{

  hspi1.Instance = SPI1;

  hspi1.Init.Mode = SPI_MODE_MASTER;

  hspi1.Init.Direction = SPI_DIRECTION_2LINES;

  hspi1.Init.DataSize = SPI_DATASIZE_8BIT;

  hspi1.Init.CLKPolarity = SPI_POLARITY_HIGH;

  hspi1.Init.CLKPhase = SPI_PHASE_2EDGE;

  hspi1.Init.NSS = SPI_NSS_SOFT;

  hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_16;

  hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;

  hspi1.Init.TIMode = SPI_TIMODE_DISABLED;

  hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_ENABLED;

    hspi1.Init.CRCPolynomial = 7;

  HAL_SPI_Init(&hspi1);

}

----------------------------------------------------------

uint8_t

CSPIN_Write_Byte

(SPI_HandleTypeDef *hspi, uint8_t byte) {

        

    // Check if SPI is running

    if((hspi->Instance->CR1 &SPI_CR1_SPE) != SPI_CR1_SPE) __HAL_SPI_ENABLE(&hspi1);

    

    /* nSS signal activation - low */

    HAL_GPIO_WritePin(GPIOC, GPIO_PIN_5, GPIO_PIN_RESET);

    

    // SPI byte send.

   hspi->Instance->DR = byte;

    

    while (__HAL_SPI_GET_FLAG(&hspi1, SPI_FLAG_BSY) == true){};            

     // nSS signal deactivation - high

    HAL_GPIO_WritePin(GPIOC, GPIO_PIN_5, GPIO_PIN_SET);         

            

        return (uint8_t)(hspi->Instance->DR);

}

-------------------------------------------------------

But it doesnt work.

As you can see in pictures, the waveforms

seem

correct

, but it does not work...

With STM32F4xx StdPeriph_Driver V1.2.0

 

(it runs fine)

0690X00000605d7QAA.png

With STM32CubeMX and HAL drivers

 

(It does not run, and MISO always returns 0x00)

0690X00000605dWQAQ.png
This topic has been closed for replies.

1 reply

Enrico Poli
ST Employee
May 21, 2015
Posted on May 21, 2015 at 08:22

Hello,

Are you sure the issue is in the firmware and not in the hardware?

According to the waveforms the MOSI is ok but in some way the MISO (SDO of the L6482) is stuck low during the transmission.

I see two possibilities:

- The L6482 is not operative

- Something (STM32?) is keeping the signal low. But in this case you'll probably damage the SDO pin of the L6482

Regards

Enrico