Skip to main content
luter
Associate III
November 23, 2005
Question

Commutation, C interrupt and C event

  • November 23, 2005
  • 3 replies
  • 611 views
Posted on November 23, 2005 at 05:26

Commutation, C interrupt and C event

This topic has been closed for replies.

3 replies

luter
luterAuthor
Associate III
May 17, 2011
Posted on May 17, 2011 at 10:19

Hi, All.

Do commutation and C interrupt occure simultaneously?

I make my question a little bit clear using next example.

Let suppose at the certain time some 3 soft priority level ISR runs. At this time MTIM rolles over MCOMP value. Let say C int has 2 soft priority level what causes pending of C int.

My question is folowing : whether real commutation occures exactly at the time when MTIM rolles over MCOMP or when C int ISR starts? And what do MCDEM and MCZEM pins show: commutation or start of ISR processing?

Tnx.

[ This message was edited by: Luter on 23-11-2005 08:42 ]

gaetano
Visitor II
May 17, 2011
Posted on May 17, 2011 at 10:19

Ciao Luter,

you are perfectly right!!.

Actually, the debug pins MCZEM and MCDEM were introduced on ST7FMC to show the exact instant when a C, D or Z event occure. This occurence is totally uncorreleted with the execution of related ISR. Moreover, a C, D and Z event cannot be masked anyway, whereas the related ISR execution can be masked acting on mask bit register.

Best regards,

Tanio

luter
luterAuthor
Associate III
May 17, 2011
Posted on May 17, 2011 at 10:19

According to my investigation Commutation and start of ISR are different events. it means Commutation can occure earlier than ISR starts. MCZEM and MCDEM pins shows commutation events.

But i would like to hear an opinion of the expert to be 100% sure.