Skip to main content
Associate II
Oct 26, 2026 12:34 PM UTC
Question

Clarification on VN9E30F IC – Channel ON and OFF Switching Feedback Register Requireemnt

Dear Sir,

We are evaluating the VN9E30F, a 6-channel automotive high-side driver with a 24-bit SPI interface. Kindly clarify whether the IC provides real-time switching status or feedback through a register that can be read via SPI.

Also, please confirm the current availability and supply status of this IC.

Thank you.

17 replies

Peter BENSCH
ST Technical Moderator
Oct 29, 2026 2:59 PM UTC

There are many registers in the VN9E30F, for example OUTCTRCR0...5, OUTCFG0...5, ADCxSR, which can be used to read the real-time status.

As the Community is a place for mutual technical support among users worldwide and thus, in a sense, a reference source, whereas questions about availability and supply status are always temporary in nature, only your preferred distributor can answer them.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate II
Oct 30, 2026 8:19 AM UTC

Dear Sir,

Thank you for your response.

As per the registers suggested by you, such as OUTCTRCR0–5, OUTCFG0–5, and ADCxSR, the actual ON/OFF status of each output channel is not directly available.

We would like to know whether an additional register is available to indicate the actual ON/OFF status (HIGH/LOW) of each output channel.

For example, in our Traffic Signal Controller application (RED, AMBER, and GREEN signals), if a particular output channel or lamp driver gets damaged or burnt, we need to identify the actual output status (HIGH or LOW) through feedback, irrespective of the internal configuration or control register settings.

Currently, we are using a separate IC to obtain the output channel feedback status. Therefore, we would like to know whether this functionality can be achieved through a dedicated status/feedback register, similar to the watchdog status register, to read the actual HIGH/LOW status of each output channel.

Best regards,
Srinivas Naik G

Associate II
Oct 30, 2026 8:20 AM UTC

We request you to kindly share the details of an authorised distributor in India for this component.

Best regards,
Srinivas Naik G

Associate
Nov 8, 2026 8:59 AM UTC

The VN9E30F provides more than simple output control. Its OUTSRx registers contain channel-specific diagnostic flags. The ADCxSR registers provide digital load-current feedback. It also supports open-load detection in ON and OFF states.

However, diagnostic feedback differs from direct voltage monitoring. For independent lamp-terminal verification, consider external voltage sensing. This helps identify actual HIGH/LOW output conditions. Validate the diagnostic thresholds against your lamp characteristics.

For IC sourcing, Unikeyic helps buyers verify MPNs, package options, datasheets, stock status, and RFQ details. They are based in Asia and sell original STM ICs. 

If you are particularly interested in buying from India, you can scroll down and run your search here.

https://www.st.com/content/st_com/en/contact-us.html

Associate II
Nov 13, 2026 1:16 PM UTC

I have gone through your reply and would like to know whether any hardware or silicon revision of the VN9E30FTR IC is planned or currently underway.

If a revision is planned, we would like to request STMicroelectronics to consider incorporating the following requirements into the revised version:

  1. Configurable Watchdog Timeout: Currently, the watchdog timeout period is fixed and cannot be configured. We would like to have an additional register to configure the watchdog timeout dynamically, with the value specified in milliseconds.
  2. Increased Load Voltage: As per our application requirements, the IC should support a load voltage of up to 36 V during normal operation. Currently, the specified maximum voltage is 28 V. Is it possible to increase the supported operating voltage to 36 V?
  3. Individual Channel Status Monitoring: We would like to have a separate register to monitor the ON/OFF status of each of the six channels, including an indication of whether each channel is functioning correctly or has failed. Currently, we are using an additional IC to implement this monitoring functionality. If this feature can be integrated into the VN9E30FTR, we could eliminate the need for the additional IC and simplify our design.

We would appreciate it if you could discuss these requirements with your technical team and let us know whether they can be considered for a future revision of the VN9E30FTR.

Associate II
Nov 13, 2026 1:28 PM UTC

Dear Sir/Madam,

We are currently using the VN9E30FTR IC from STMicroelectronics in our product development activities. However, we are unable to find this component available for purchase through major online distributors such as Digikey, Mouser, and element14.

We would like to obtain clarification regarding the availability and product lifecycle status of this IC. Kindly provide information on the following:

  1. Current Availability: When is the VN9E30FTR IC expected to be available for purchase? Is there any current supply constraint or lead-time issue?
  2. Product Continuity: Is STMicroelectronics planning to continue manufacturing and supplying this IC, or is there any plan to discontinue the product?
  3. Product Revision: Is any hardware or silicon revision planned or currently underway for this IC?
  4. End-of-Life (EOL) Status: Has an EOL announcement been made or is the product expected to reach EOL in the near future? If so, kindly share the expected timeline.
  5. Future Supply: Can you support our future procurement requirements and provide an estimated lead time and minimum order quantity?

As this IC is an important component in our ongoing product development, understanding its long-term availability and lifecycle status is essential for our design and procurement planning.

We would appreciate it if you could check with STMicroelectronics and share the latest information.

Thank you for your support.

Peter BENSCH
ST Technical Moderator
Nov 16, 2026 2:45 PM UTC

​@SrinivasNaikG The community is a place for mutual technical assistance among users, so that all users can benefit from answers given here.

Questions about current and future availability are, however, always temporary, so you would need to clarify them with your preferred distributor.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate II
Nov 17, 2026 4:19 AM UTC

I have gone through your reply and would like to know whether any hardware or silicon revision of the VN9E30FTR IC is planned or currently underway.

If a revision is planned, we would like to request STMicroelectronics to consider incorporating the following requirements into the revised version:

  1. Configurable Watchdog Timeout: Currently, the watchdog timeout period is fixed and cannot be configured. We would like to have an additional register to configure the watchdog timeout dynamically, with the value specified in milliseconds.
  2. Increased Load Voltage: As per our application requirements, the IC should support a load voltage of up to 36 V during normal operation. Currently, the specified maximum voltage is 28 V. Is it possible to increase the supported operating voltage to 36 V?
  3. Individual Channel Status Monitoring: We would like to have a separate register to monitor the ON/OFF status of each of the six channels, including an indication of whether each channel is functioning correctly or has failed. Currently, we are using an additional IC to implement this monitoring functionality. If this feature can be integrated into the VN9E30FTR, we could eliminate the need for the additional IC and simplify our design.

We would appreciate it if you could discuss these requirements with your technical team and let us know whether they can be considered for a future revision of the VN9E30FTR.

Peter BENSCH
ST Technical Moderator
Nov 17, 2026 7:39 AM UTC

Your request for additional registers or an adjustment of the watchdog for an already existing component would change compatibility with the current device and would require a new device. Please share your expected annual demand for such a device with your local distributor so that they can initiate the next steps.

 Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate II
Nov 17, 2026 8:19 AM UTC

Current Availability: When is the VN9E30FTR IC expected to be available for purchase?

Peter BENSCH
ST Technical Moderator
Nov 17, 2026 10:38 AM UTC

You have asked this question before. Please, let me repeat my previous answer once again:

Questions about current and future availability are, however, always temporary, so you would need to clarify them with your preferred distributor.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate II
Nov 17, 2026 10:46 AM UTC

Is there an option available for me to provide feedback about your services? I would like to share some suggestions for improvement.

Associate II
Nov 17, 2026 10:49 AM UTC

It is currently out of stock across all major online distributors, including DigiKey, element14, Mouser, and others.

Peter BENSCH
ST Technical Moderator
Nov 18, 2026 7:22 AM UTC

We are currently seeing strongly increasing worldwoide demand, which may in some cases lead to longer delivery times. For specific information on availability, as mentioned, your contact person at your local distributor is best placed to help you further.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Visitor II
Nov 18, 2026 7:51 AM UTC

You could check out spacechips.tech; they have COC certificates and stock available.

Associate II
Nov 18, 2026 8:50 AM UTC

kindly share the link for purchase or procurement?