Skip to main content
Visitor II
August 1, 2025
Question

Clarification on STUSB4710QTR Configuration for 5V/5A Power Source

I just need some clarification regarding the STUSB4710QTR.

I'm designing a USB-C power source where a USB 2.0 hub will supply 5 V/5 A to a USB device. The connected device is a USB cellular modem, which typically draws a continuous 5 V/3 A, but requires brief pulses of up to 5 V/5 A during transmission.

I would like to configure the SEL_PDO pin for this application without using I²C. Could you please confirm if there is a default PDO profile that supports this, or if the SEL_PDO configuration allows selecting a 5 V/5 A contract directly?

I've attached a reference for your review.
Please let me know if everything looks in order or if you have any recommendations.

Thank you in advance for your support.

This topic has been closed for replies.