Skip to main content
Associate
August 14, 2024
Question

Choosing right transformer

Hi,

I want to design AC-DC converter using VIPER26H. The suitable development board is STEVAL-ISA081V1 which is based on VIPER26L. Can someone help me to find a transformer manufacturing part no.? I want 12V 10W output.

This topic has been closed for replies.

1 reply

Peter BENSCH
ST Technical Moderator
August 14, 2024

The transformer used in the STEVAL-ISA081V1 was developed in 2010 for use with the VIPER26L (60kHz); the 760871131 from Wuerth Elektronik is very similar.

However, the VIPER26H operates at the higher frequency of 115kHz, for which the transformer must be designed. If you don't want to have a customised transformer made, you could try the 750310849, which was designed for a switching frequency of 132kHz. Wuerth Elektronik or another transformer manufacturer will be happy to help you with your choice.

Hope that helps?

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.