Skip to main content
Visitor II
March 25, 2026
Question

Charge Controller suggestion to Charge lifepo4 Battery 80A

Hi,

We are looking for recommendations on a suitable topology and charge controller for charging a LiFePO₄ battery with the following requirements:

Input voltage: 9–36 VDC

Output voltage: 10–36 VDC

Output current: up to 80 A

We understand that a single IC may not support this current level, so we are considering a parallel architecture using multiple controllers. Kindly suggest an appropriate approach and suitable IC options.

Thanks,
BK