Skip to main content
glubschi_sp
Associate II
January 12, 2005
Question

Changing the PWM-Frequency at runtime

  • January 12, 2005
  • 3 replies
  • 864 views
Posted on January 12, 2005 at 07:15

Changing the PWM-Frequency at runtime

This topic has been closed for replies.

3 replies

gaetano
Visitor II
May 17, 2011
Posted on May 17, 2011 at 10:18

Hi,

it is possible to change the PWM frequency runtime as you are saying. If you open the ST7MC datasheet at page 196 ''PWM Generator Block'' paragraph, you will find how the system works.

Best regards,

Tanio

glubschi_sp
Associate II
May 17, 2011
Posted on May 17, 2011 at 10:18

Hi,

I'm use the St7FMC2N6B6 controller in an inverter. Is it possible to change the PWM-frequency while the motor is running? Have the outputs to be seperated? Or can I change the PWM counter prescaler without stopping the outputs?

Are the corresponding bits in the ARTCSR Register (Bit CC[2..0])?

Best regards,

Micha

glubschi_sp
Associate II
May 17, 2011
Posted on May 17, 2011 at 10:18

Thank you very much for your fast help!

That means, a adaptive PWM-frequency is possible, to reduce powerlosses in the powermodule. Not bad!

Best regards,

Micha