Skip to main content
mustafacmk
Associate
July 12, 2018
Question

Can the high voltage L9907 Driver Circuit be installed?

  • July 12, 2018
  • 0 replies
  • 484 views
Posted on July 12, 2018 at 16:39

I want to do a motor drive with the l9907. I have STP315N10F7 Mosfet. But there is a problem. The driver says that it supports up to 54V, but I want to use the MOSFET drain pin with 85V. How can I do that?

#motor-control #motor-driver-ic
This topic has been closed for replies.