Skip to main content
AJuki.1
Associate
April 28, 2021
Question

Can STEVAL-SPIN3201 be programed for 6step?

Hi,

I was wondering, if you can programm STEVAL-spin3201 board to 6-step mode, instead of FOC?

This topic has been closed for replies.

5 replies

Cristiana SCARAMEL
ST Employee
May 3, 2021

Hello @AJuki.1​ and welcome to the ST Community.

Yes, you can use the STEVAL-SPIN3201 board to drive a motor with 6-step method.

You can find a firmware example in the last release of STM32 Motor Control SDK (X-CUBE-MCSDK-Y).

With this example you can perform a 6-step control in voltage mode and with Hall sensor for speed feedback.

Let me know if this info is useful to you, if yes please "Select as Best" button to close the topic.

"If you feel a post has answered your question, please click ""Accept as Solution"""
Associate III
December 6, 2023

can you help me which version is useful for six-step method. 

Cristiana SCARAMEL
ST Employee
December 18, 2023

Hello @vishu the proper label for questions about STM32 Motor Control SDK is STM32 MCUs Motor Control.

I’ve seen that there are already your open topics on the subject, please do not spam.

"If you feel a post has answered your question, please click ""Accept as Solution"""
AJuki.1
AJuki.1Author
Associate
May 4, 2021

Hello,

thank you for your answer. The firmware example worked, but the problem is that it is not rotating, It is stuck and shakes like crazy. Is it maybe a problem between rotor and magnetic field, not being in sync?

Cristiana SCARAMEL
ST Employee
June 17, 2021

Hi @AJuki.1​,

sorry for late reply. Did you solved your issue?

Do you confirm that you want perform a 6-step control in voltage mode and with Hall sensor for speed feedback?

Otherwise there is also the example of 6-step control in voltage mode and sensorless.

Moreover, I suggest the check the following points according to your requirements:

  • the board jumpers configuration
  • the motor parameters (pole pairs, target speed, ...)
  • the sensors commutation table (If the sequence of commutation of the Hall sensors is not standard, the firmware has to be edited according to your table).

Let me know the progress about your project.

"If you feel a post has answered your question, please click ""Accept as Solution"""