Skip to main content
WEmme
Associate
September 12, 2019
Question

Can STEVAL_POE002V1 work as 24V source?

  • September 12, 2019
  • 1 reply
  • 704 views

I bought the STEVAL_POE002v1. It works fine at 5 V. Now I want to setup a POE with 24V. Can I achieve this with that STEVAL? I would think to change the transformer and to adjust the Feedback-path and perhaps the Fsw. Can you help me with a calculation example like an Excel sheet or something else?

Many thanks in advamnce!

Best regards

Wolfgang

This topic has been closed for replies.

1 reply

WEmme
WEmmeAuthor
Associate
September 12, 2019

Additional question: Do you recommend another STEVAL_*** for this?

Regards

Wolfgang