Skip to main content
Associate
June 3, 2025
Solved

can PG pin of ST1L08SPU33R be left floating if unused?

can PG pin of ST1L08SPU33R be left floating if unused?

Datasheet does not specify it.

 

 

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
June 3, 2025

This is also stated in the data sheet, table 2: VPG = -0.3V ... VBIAS+0.3V. So, pull it to VBIAS.

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

7 replies

Peter BENSCH
ST Technical Moderator
June 3, 2025

Welcome @shubhangi, to the community!

It is indeed mentioned a little hidden. However, the data sheet, table 4, states Isink = 6 mA open drain output for PG. This pin is therefore an open drain output and can therefore remain completely unconnected.

Hope that answers your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
shubhangiAuthor
Associate
June 3, 2025

Hi Peter,

Thank you for your response. It indeed is hidden. :) 

If I want to use this pin, I assume, I will have to pull-this up. Which voltage rail should it be pulled-up to?

 

Thanks,

Shubhangi

 

 

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
June 3, 2025

This is also stated in the data sheet, table 2: VPG = -0.3V ... VBIAS+0.3V. So, pull it to VBIAS.

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
shubhangiAuthor
Associate
June 3, 2025

Thanks Peter.

 

Regards,
Shubhangi

shubhangiAuthor
Associate
June 20, 2025

Hello Peter,

Can this IC ST1L08SPU33R handle 3.3V input? i.e. convert 3.3V to 3.3V?

Actually I have a case where input can be either 3.3V or 5V. 5V to 3.3V can work. How about 3.3V to 3.3V?

Thanks,

Shubhangi

Peter BENSCH
ST Technical Moderator
June 20, 2025

Well, it is an ultra low drop regulator, but there is still some dropout voltage: the data sheet mentions max 120mV for the whole temperature range, in your case resulting to 3.18V.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
shubhangiAuthor
Associate
June 20, 2025

Hi Peter,

Yes Thats expected. I think 3.18V should work. Thanks.

Thanks,
Shubhangi