Solved
Benoit FORETBest answer
ST Employee
Jan 7, 2019 4:00 PM UTC
Hello,
thanks for your schematic. I reviewed with the application team and there are indeed a couple of feedbacks we'd like to share with you. Would you mind sharing your email address through direct messaging? (click on my name from this discussion and then MESSAGE button).
To answer you question:
- Yes, as far as you can access SDA, SCL and GND from your board, then you will be able to connect it to the NUCLEO-F072RB in order to interconnect with the GUI (STSW-STUSB002)
- To program the STUSB4500 with the GUI, it can run only with STSW-STUSB002 so far. But you can do it also using the software library (STSW-STUSB003) which can be quite easily compiled on any MCU, especially if STM32.
Benoit