Skip to main content
CVT.1
Visitor II
Sep 15, 2020 4:29 AM UTC
Solved

Can I get any application note on STGPIN3H60 with wave form requirements ,the permitted frequency limits etc.

..

This topic has been closed for replies.
uomo motore
uomo motoreBest answer
Associate
Sep 16, 2020 3:53 AM UTC

This info is already available in the datasheet. It has the max frequency limit in the table. There are timing diagrams related to interlocking for the PWM inputs and also for the SmartShutdown function including application information. Do you have any specific query?​

2 replies

uomo motore
uomo motoreBest answer
Associate
Sep 16, 2020 3:53 AM UTC

This info is already available in the datasheet. It has the max frequency limit in the table. There are timing diagrams related to interlocking for the PWM inputs and also for the SmartShutdown function including application information. Do you have any specific query?​

Cristiana SCARAMEL
ST Employee
Sep 24, 2020 8:30 AM UTC

Hi @CVT.1​,

the @uomo motore's​ answer solved your doubts?

If yes please "Select as Best", otherwise as abovementioned do you have any specific query?

"If you feel a post has answered your question, please click ""Accept as Solution"""