Skip to main content
huaer2000
Associate III
May 23, 2005
Question

Can i delete the prepositioning phase while using St7MC?

  • May 23, 2005
  • 2 replies
  • 700 views
Posted on May 23, 2005 at 06:08

Can i delete the prepositioning phase while using St7MC?

This topic has been closed for replies.

2 replies

gaetano
Visitor II
May 17, 2011
Posted on May 17, 2011 at 10:18

Dear sir,

the prepos phase is essential to have the best motor start-up in a sensorless system.

If, theoretically, you eliminated this stage, you could have in any case a reverse rotation, due to a not well-known rotor position, and, even worst, you could fail at all the motor start-up, causing a sudden rotor-blocked condition.

So, in my opinion you should kept the alignment phase...

Regards,

Tanio

huaer2000
huaer2000Author
Associate III
May 17, 2011
Posted on May 17, 2011 at 10:18

Dear sir,

Now I want to delete the prepositioning phase whilse using st7MC for sensorless control in open loop mode, Can I do like that? becasue you know, with prepositiong phase the motor maybe move reversely in the start-up. Thanks the help!

mcuintereest