Skip to main content
paul16
Associate
Sep 25, 2009 6:14 PM UTC
Question

calculating acceleration ramp table

Posted on September 25, 2009 at 20:14

calculating acceleration ramp table

This topic has been closed for replies.

2 replies

paul16
paul16Author
Associate
May 17, 2011 8:16 AM UTC
Posted on May 17, 2011 at 10:16

HI

we are using the ST7FMC micro in our application and all the sample code is generated using the GUI however in our app we will need to be able to update the Acceleration ramp can someone point me to an app note or give me information on the equation used to calculate the ramp within the GUI so we can do the same in our app.

Thanks In advance

tomas23
Visitor II
May 17, 2011 8:16 AM UTC
Posted on May 17, 2011 at 10:16

Hi Paul, if I remeber well, the speed ramp has first been evaluated in Excel, but I am not sure whether this is still available.

In forced mode during start-up only commutation event delay and the timer prescaler have been updated, you can easily calculate the speed from these two parameters (or vice-versa, calculate the tim prescaler and commutation delay from required speed -or step time-)