Skip to main content
DSHAR.31
Associate II
March 21, 2024
Question

Burning of resist. R154 of PM8834 auxiliary power to MOSFET driver of PFC of STDES-3KWTLCP ref dsgn

I have assembled PFC and LLC circuit of STDES-3KWTLCP reference design. I followed the procedure as described in the document to assemble whole circuit. When we gave AC voltage to PFC, resistance R154 gets heat up and eventually burn out. I double checked all the components value and their placement but couldn't find the cause for this behavior.

Can anyone please assist us in finding which part of the circuit or component is creating this issue so that it would help us in rectifying the cause?

 

Thanks.

This topic has been closed for replies.

19 replies

Peter BENSCH
ST Technical Moderator
March 21, 2024

Well, if R154 gets too hot, there will obviously be too much current flowing through it. Please check C161 and its insulation. Then also check the signals on PWM1, PWM2 and OUT1, OUT2 on U105.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
DSHAR.31
DSHAR.31Author
Associate II
March 23, 2024

I changed C161 and checked PWM1, PWM2,  OUT1 and OUT2 of U105 with No Load connected. All these 4 pins have PWMs on them. Still, R154 is heating too much.

AScha.3
Super User
March 23, 2024

Check generated voltages : VCC_+ 18A + 18B + 12 V  . ok?

If you feel a post has answered your question, please click on " Best Answer ".
DSHAR.31
DSHAR.31Author
Associate II
March 26, 2024

Voltages are also OK.

DSHAR.31
DSHAR.31Author
Associate II
March 30, 2024

Is there anything I can check to find the cause of this issue?

AScha.3
Super User
March 30, 2024

What i would do (at work) : look with a IR-camera , to see, whats getting suspicious "warm" ...

If you dont have this : the small transformer makes 3 outputs: VCC_+ 18A + 18B + 12 V ;

(minimum) one of them using too much power, so R154 gets hot.

Find out, where something gets hot, or where the power is going to.

If you feel a post has answered your question, please click on " Best Answer ".
DSHAR.31
DSHAR.31Author
Associate II
March 30, 2024

We already checked with the IR-camera. Only  R154 gets suspiciously warm (temp. reaches to around 100 deg celsius). Rest all circuit remains cool. We also disconnected the MOSFET driver IC (U101 and U102) which runs by these 3 outputs. The purpose of removing the connection to U101 and U102 is to check whether R154 gets heated despite not being connected to any load. After doing this, only R154 gets too hot when looked by IR-camera.

Peter BENSCH
ST Technical Moderator
April 3, 2024

If you get a voltage of 50V at VCC_+18VA after removing D112, the maximum reverse voltage of one or all Schottky of the bridge rectifiers will be too low. Either replace the bridge rectifiers with 60V or 80V Schottky, as @AScha.3 suggested, or with ultrafast rectifiers with >80V.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
DSHAR.31
DSHAR.31Author
Associate II
April 6, 2024

Just to be sure that the issue is not with auxiliary supply, I removed the auxiliary circuit and gave all 3 VCCs externally using 3 different regulated power supply (2 X 18V and 1 X 12V).

What I observed is , both gate drivers STGAP2D  draws too much current that one of them burnt with flames, while other one also got damaged completely, with external VCCs dropping to 2V for 12V and 9V for 18V..

 

I still cannot understand which section is wrong.

 

AScha.3
Super User
April 6, 2024

Upps...now no need to understand which -- now repair ALL .

You have to replace all gate drivers, and when removed the old, check gates of mosfet/igbts for good or dead (most time short or low resistance, if damaged).

Was this 3kW inverter running ever ? What happened before ? 

If you feel a post has answered your question, please click on " Best Answer ".
DSHAR.31
DSHAR.31Author
Associate II
April 7, 2024

Only once we got output as 400V from this PFC. But this output remained for only couple of seconds and R154 got burnt. 

After replacing R154, it got burnt several times but 400V output never came and MOSFET also got shorted couple of times.