Skip to main content
Visitor
Nov 9, 2026 8:35 AM UTC
Question

BTB04-600SL: Is marking BTB04600SL (without dash) the same part as BTB04-600SL?

Hi ST team,

We received batches of BTB04-600SL triacs with two different body markings:

  1. Marked: BTB04-600SL
  2. Marked: BTB04600SL (no dash separator)

Could you help confirm:

  1. Are they electrically identical, same die and specification?
  2. Is the dash "-" optional for component laser marking?

Best regards

L Ma

1 reply

Peter BENSCH
ST Technical Moderator
Nov 9, 2026 9:01 AM UTC

Welcome ​@Lma, to the community!

You have not included any photos, so it is not even possible to do a rough check for fakes among them, but I can confirm that the BTB04-600SL is produced at several sites that apply the marking with exactly this difference. So if it is demonstrably genuine original goods, there are no technical differences whatsoever between the version with the dash and the one without the dash.

Hope that answers your questions?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.