BTA16-600BW not turning off
Hi
I have been testing the following circuit (which apparently works). I am finding that the TRIAC (BTA16-600BW) does not turn off with an inductive load (induction motor at 240V, 3A. 50Hz) yet with a simple house lamp the circuit works switching the lamp on and off.
I have modified R9 to 360ohm (340V/1A = 340ohm) chose 360
R10 has also been modified to 360ohm
R39 was added at 510ohm
I have removed L3, C11 and C13 from the circuit.(they are for EMI)
I have swapped MT1 and MT2 so that active is now on TRIAC pin 2 and TRIAC pin 1 feeds the load.
Though this is a snubberless part I added a snubber, 560ohm 0.1uF
none of these changes make a difference.
I turn the relay on which provides power.
I turn the OPTO on which turns the TRIAC on, but when I turn the OPTO off again the motor slows a little but does not stop.
OPTO is MOC3021
Either the OPTO or TRIAC is latching on and remaining on at the zero crossing. A snubber is supposed to improve this. Maybe my values are way off.
Any suggestions?
Thanks
Andre