Skip to main content
aengelhardt
Associate
July 16, 2004
Question

Brushless 1-phase motorcontrol

  • July 16, 2004
  • 2 replies
  • 612 views
Posted on July 16, 2004 at 10:45

Brushless 1-phase motorcontrol

This topic has been closed for replies.

2 replies

gaetano
Visitor II
May 17, 2011
Posted on May 17, 2011 at 10:17

Hello,

for me it isn't clear how a triac can be used for controlling a BLDC motor. Generally this switch is used when we deal with AC motor or universal motor. I would appreciate more details about your system, i.e., the architecture of your driver (micro or not?) and the type of motor (application field, size, power, etc.).

Regards,

Tanio

aengelhardt
Associate
May 17, 2011
Posted on May 17, 2011 at 10:17

Hello,

is there anybody who can give me some hints (or more

) for a design of a 1-phase BLDC Motor? (yes, 1-phase)

I need a very low noise control.

The current solution ist running with a triac. But the triac becames very loud if the motor runs slow.

App-Notes or something like that would be very helpfull.

Thx in advanced