Skip to main content
Aidan Walton
Visitor II
June 27, 2018
Question

Bi-polar outputs using SRK2000A?

  • June 27, 2018
  • 0 replies
  • 539 views
Posted on June 27, 2018 at 12:26

Hi,

I've almost completed the design of a 150W 35-60V Input and +15 / -15V Output DC-DC LLC resonant converter using L6599. On the secondary side I have a center tapped winding configured across a full bridge to deliver +15V and -15V, with the center tap as my floating GND. The rectifier diodes are consuming considerable power, rather hot. I have clearly tried schottkys but still rather hot. I could try FERD rectifiers, which will bring power dissipation down to just a couple of watts. However this is a battery powered application so power efficiency is important.

I would like to try using the SRK2000A with MOSFETs, however I don't see any applications where the controller is used with a bi-polar output.

Is it possible to configure the SRK2000A to full bridge rectify and produce +15V and -15V from a center tapped secondary?

#dc-dc #synchronous-rectification #srk2000a #bipolar-output
This topic has been closed for replies.