Skip to main content
STLearner
Associate III
April 24, 2023
Question

Battery charger solution

Hi ST experts,

Would like to know if ST has any recommendation on battery charging solution?

The battery pack requirement is 7.4V 2300mAH which is 2-cells construction.

The intention is to change from standalone battery charger IC to a smart charger solution whereby it can help to prolong the battery lifespan for example having trickle charging and battery health (SOC) to keep the battery charge to max 80% (this can be done by configurable through software or hardware) and depth of discharge to 50% or 25%

Appreciate with any suggestions which can meets above-mentioned requirements.

Thanks.

    This topic has been closed for replies.

    1 reply

    Winfred LU
    ST Employee
    April 25, 2023

    Sorry. There is no solution fitting the requirements.

    Battery charger portfolio:

    https://www.st.com/en/power-management/battery-chargers.html