Skip to main content
jones23
Associate III
August 2, 2007
Question

AN2281's problem.

  • August 2, 2007
  • 2 replies
  • 606 views
Posted on August 02, 2007 at 08:13

AN2281's problem.

This topic has been closed for replies.

2 replies

gaetano
Visitor II
May 17, 2011
Posted on May 17, 2011 at 10:14

Hi Ferrari,

that solution is not suitable for DC voltage different from 12V.

For ''Low Voltage'' motor control application (I mean from 6V up to 48V) it will be delivered a demokit that makes use of HVIC driver L6387, PowerMOS (with the possibility to use different devices at different current ratings) and ST7MC as microcontroller. The system is under beta testing and will be soon available in ST site.

Regards,

Tanio

jones23
jones23Author
Associate III
May 17, 2011
Posted on May 17, 2011 at 10:14

Dear TANIO sir..

AN2281 design for 12V or Low voltage 3PH system. Can I use in AC110V 3PH system? I have been test HVIC + MOS. But Always broken. Can you give me some advice. THANKS~~

Best Regards

Ferrari