Skip to main content
Explorer
February 27, 2025
Solved

About the TS3330AMR

The TS3330AMR has a voltage reference, but the internal configuration of the IC is unclear.
Is a reverse bypass diode, like the reverse voltage protection of a linear regulator, unnecessary?

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
February 27, 2025

Welcome @Ikegawa, to the community!

Well, the data sheet clearly states in the absolute maximum ratings (table 1):

VOUT (Maximum voltage on the output pin) -0.3V to VIN +0.3V

So if the input voltage drops to zero and the output voltage of 3V is still present at the output due to large capacitors, for example, the max rating is violated without the Schottky diode mentioned.

Hope that answers your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
February 27, 2025

Welcome @Ikegawa, to the community!

Well, the data sheet clearly states in the absolute maximum ratings (table 1):

VOUT (Maximum voltage on the output pin) -0.3V to VIN +0.3V

So if the input voltage drops to zero and the output voltage of 3V is still present at the output due to large capacitors, for example, the max rating is violated without the Schottky diode mentioned.

Hope that answers your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.