Skip to main content
huaer2000
Associate III
September 8, 2004
Question

about st7mc problem

  • September 8, 2004
  • 2 replies
  • 510 views
Posted on September 08, 2004 at 06:14

about st7mc problem

This topic has been closed for replies.

2 replies

huaer2000
huaer2000Author
Associate III
May 17, 2011
Posted on May 17, 2011 at 10:17

dear sir,

I want to drive a bldc motor in sensorless mode with st7mc. but because

I use IR2103 as driver now I have to change the source code. Now I want to

know if there are any other places I have to change the source code except for MPOL and MPWME?

best regards,

mcuinterest
gaetano
Visitor II
May 17, 2011
Posted on May 17, 2011 at 10:17

Hi,

ok to change MPOL register due to the fact that the low side input of the driver is active LOW. But, it isn't clear for me why you have to manage also the MPWME register?

Waiting your answer,

Tanio