Skip to main content
MScho.10
Visitor II
Aug 24, 2020 11:44 PM UTC
Question

X-CUBE-EEPROM missing GetBankNumber() definition for STM32G474

In the X-CUBE-EEPROM library (https://www.st.com/en/embedded-software/x-cube-eeprom.html)

FLASH_OPTR_BFB2 is defined for the stm32g474 in

Drivers/CMSIS/Device/ST/STM32G4xx/Include/stm32g474xx.h

and therefore the following in

Middlewares/ST/EEPROM_Emul/Porting/STM32G4/flash_interface.c is also defined.

```

uint32_t bank = FLASH_BANK_1, page_error = 0U;

#if defined(FLASH_OPTR_BFB2)

  bank = GetBankNumber(PAGE_ADDRESS(Page));

#endif

```

however, GetBankNumber() is only defined in the L4 and L5 flash_interface.c files. It does not have a function definition in the .../STM32G4/flash_interface.c

This seems like a bug in X-CUBE-EEPROM. Is there a way to report this bug directly? or anyone know of a fix for it? just commenting out "bank = Get..." gets it to compile, though I have not tested if this actually works yet.

This topic has been closed for replies.

1 reply

ST Technical Moderator
Aug 28, 2020 12:43 PM UTC

Hello @MScho.10​ ,

Thank you for your reported issue.

I raised this internally to the appropriate team for correction and adding definition of GetBankNumber().

Best Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks