Skip to main content
MÇETİ.1
Associate III
Aug 9, 2022 10:42 AM UTC
Question

while launching new project, libraries file does not exist

Hi everyone, I'm tryin to learn how to use stm32f4 boards. But I have a problem when I create new project libraries file doesn't exist as it was. I did not see problem like this before while using stm32f1xx series, and also there is a warning like this. Please help me0693W00000QNI1gQAH.png

This topic has been closed for replies.

2 replies

mattias norlander
ST Technical Moderator
Aug 15, 2022 4:57 PM UTC

Looks like you are using TrueSTUDIO. Not STM32CubeIDE right?

The warning you see is because the local varliable data is not used in this function. Not necessarily a problem when executing the example. More a remark that the code could be improved...

I don't understand what you mean with:

"But I have a problem when I create new project libraries file doesn't exist as it was. I did not see problem like this before while using stm32f1xx series".

In your screenshot I don't see any error at all.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Tesla DeLorean
Guru
Aug 15, 2022 5:41 PM UTC

Is the variable used or not?

Warnings are there to be informative, in case you missed something, or that the logic eliminates things.

The code may be a hold over from a prior iteration, or be there for a different build option, we other code is taken or ignored based on a top level define, or build for Debug vs Release.

Learn to differentiate Warnings from Errors

Learn to read/walk Code, and discern intent.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..