Skip to main content
David.Cheng
Associate III
Aug 4, 2019 5:37 AM UTC
Question

what will happen if a function has many lines in KEIL MDK 5

i have called a function big , and then found some memory overwrite

This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
Aug 4, 2019 12:56 PM UTC

Automatic/Local variables reside on the stack, make sure it is adequate for function and everything it calls directly and indirectly. Check size, defined in startup_stm32xxxx.s​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
David.Cheng
Associate III
Aug 4, 2019 1:14 PM UTC

thanks ! i will large it by which rule

Tesla DeLorean
Guru
Aug 4, 2019 6:18 PM UTC

Not sure I fully comprehend the response. The routines will use space dependent on your code, understand the memory foot-print of what you're expecting to be allocated. There is a direct cause and effect, if you have 4KB of structures/arrays it has to come from somewhere. One could measure maximal depth by filling the available stack area with a recognizable pattern, and then inspecting with a memory view in debugger. Or have code to measure how much of the pattern remains.

This is not a specifically STM32 or Keil issue, but a general C and micro-controller one.

GNU/GCC hides this somewhat as it puts the stack at the top of available RAM in the STMicro scripts, whereas Keil gives it a defined size, and resides above the heap, locale and statics.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..