Skip to main content
Rinoue
Associate
Sep 12, 2020 3:13 PM UTC
Solved

What is the digital pins's frequency of Nucleo-f303K8?

I tried to find the frequency that the digital ports of Nucleo-F303k8 can accept data (example: the arduino works with 10kHz on these pins), but i couldn't find anywhere. Someone can help me? I need to use some sensors and I need this information to but them.

This topic has been closed for replies.
TDK
TDKBest answer
Sep 13, 2020 2:30 PM UTC

Well, it's not super clear what you're asking as "can accept data" is pretty vague. If you're asking about maximum speed the GPIO pins can switch, it can be found in "Table 53. I/O AC characteristics". Maximum SPI/I2C speeds can be found in the very first sentence of their respective sections.

"If you feel a post has answered your question, please click ""Accept as Solution""."

7 replies

TDK
Sep 12, 2020 8:56 PM UTC

That info will be in the datasheet. They can generally drive or be driven by signals of tens of MHz without issue, but consult the datasheet if you need details.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Rinoue
RinoueAuthor
Associate
Sep 13, 2020 2:23 PM UTC

I couldn't find it in the datasheet. I'm noob in eletronics in general and I dont undestand where I can find these things on datasheet, can you help me?

TDK
TDKBest answer
Sep 13, 2020 2:30 PM UTC

Well, it's not super clear what you're asking as "can accept data" is pretty vague. If you're asking about maximum speed the GPIO pins can switch, it can be found in "Table 53. I/O AC characteristics". Maximum SPI/I2C speeds can be found in the very first sentence of their respective sections.

"If you feel a post has answered your question, please click ""Accept as Solution""."
waclawek.jan
Super User
Sep 13, 2020 8:02 AM UTC

> the arduino works with 10kHz on these pins

Where do you have this information from?

JW

Rinoue
RinoueAuthor
Associate
Sep 13, 2020 2:17 PM UTC

I found this on a forum from Arduino, but i dont have the link

MM..1
Super User
Sep 13, 2020 2:29 PM UTC

this way you dont find finish...

try write how sensor how bus.

For example SPI can clearly work on 25MHz...