Skip to main content
Associate II
Nov 5, 2026 1:16 PM UTC
Question

What ESD protection to use for STM32G051

I’m using a STM32G051 with a PS/2 Mouse that is powered by 5V.

 

I don’t know how to find out the max voltage that the STM32G051 can experience from a temporary ESD surge before it gets damaged. 

I can’t find the TLP anywhere.

I’m not sure what the clamping voltage should be for the TVS diode.

 

 

3 replies

Andrew Neil
Super User
Nov 5, 2026 2:25 PM UTC

I don’t know how to find out the max voltage that the STM32G051 can experience from a temporary ESD surge before it gets damaged. 

Look at the Absolute Maximum ratings ?

Those specify conditions beyond which damage may occur...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
CYANG.1
ST Employee
Nov 6, 2026 2:12 AM UTC

Hi,

 

You can refer to ESD specification of STM32G5 in datasheet as shown below.

 

LCE
Principal III
Nov 6, 2026 6:26 AM UTC

… which basically means that there is no real in-built protection - which is quite normal for non-interface ICs.

 

If you only expect “some minor ESD” from connecting stuff, you might get away with a few small TVS in SOT23 or other SMD.

Check the capacitance of the TVS, in relation to the interface speed.

If possible also add some serial resistors or ferrite beads.

And even more important: think about where the energy of an ESD pulse might go, it doesn’t simply disappear by inserting some protection carelessly. Even if nothing gets damaged, resets and stranger things might happen.
So try to “guide” it to the device’s case (or some other “bulk capacitance” (not finding the right words in english)), keeping it separate from the PCB GND.