Skip to main content
PPopo
Associate III
Nov 26, 2020 9:03 AM UTC
Question

Using Arduino Uno as USB to serial converter

Hello,

I have an STM32 Nucleo-64 board with STM32F446RE MCU.

I want to talk to it's native bootloader stored in system memory and play around with it a bit(do some in application programming, etc) via the demonstrator program.

Since the bootloader communicates via USART1/SPI1/etc I need an usb to usart/spi converter to serve as interface between my PC and the board.

I don't have a converter around atm, I do however have an arduino uno.

Would it be possible to use it simply as an USB to usart converter so I can use the demonstrator to talk to the native bootloader on the STM board's MCU? Has someone ever used an arduino in this fashion?

Thank you!

This topic has been closed for replies.