Skip to main content
Associate II
Jan 27, 2024 12:43 PM UTC
Question

"Unknown signal" when trace GPIO pin status in Keil5 logic analyzer (Nucleo-H743ZI2)

Hello,

I try to trace the GPIO pin status in Keil5 MDK ARM logic analyzer, but it's not successful.

I am using the Nucleo-H743ZI2 board with STLink 3 SWO mode. I can also see the printf output in the "Debug (printf) Viewer" without any issue. The LED on board is on PB0. In the debug mode, I can see the GPIOB ODR is updating, which aligns with the LED status.

But when I type the "PORTB.0" in the Logic Analyzer setup, it said "Unknown signal".

Is there a way to trace the GPIO pin status in the logic analyzer by Keil5 MDK ARM? I tried "PORTB.0", "GPIOB.0", etc, but none of them works.

屏幕截图 2024-01-27 202501.png

Thanks in advance.

BR,

JN  

This topic has been closed for replies.

1 reply

Andrew Neil
Super User
Jan 27, 2024 1:12 PM UTC

Note that Keil Tools are from an independent company - nothing to do with ST.

For questions about the Keil tools, try:

https://community.arm.com/support-forums/f/keil-forum

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.