Skip to main content
Associate
Nov 18, 2025 8:14 AM UTC
Question

unable to get output in 3.5"tft spi display having ili9488 driver

I am currently working on a project using the STM32F401RE Nucleo board interfaced with a 3.5-inch TFT SPI display (ILI9488 driver). I am facing an issue where the display does not show any output, even though the backlight turns on and the code uploads successfully without errors.

I have already checked the SPI connections, power supply, and display initialization code, but the screen still  remains blank. I would like to kindly request your guidance or any reference materials/libraries that can help me correctly configure and test the display with STM32CubeIDE.

If possible, I would appreciate help with:

  • Correct SPI configuration for ILI9488

  • Required GPIO pin mapping (DC, RESET, CS, etc.)

  • A working example code or initialization sequence

  • Any known issues or recommended libraries for STM32F4 + ILI9488

Your support will greatly help me continue my project. Thank you

This topic has been closed for replies.

5 replies

AScha.3
Super User
Nov 18, 2025 1:21 PM UTC

The SPI settings...i can tell you later, at home.

But first: i found, some waiting time after release reset line to TFT is needed; so try with hal_delay(50) , before sending anything to the ILI .

If you feel a post has answered your question, please click on " Best Answer ".
AScha.3
Super User
Nov 18, 2025 6:23 PM UTC

SI setting...is for ILI9344, so check: same (or not) for 9488 ...

AScha3_0-1763489745821.png

+

here a lib, if your lib has problems:

https://github.com/RobertoBenjami/stm32_graphics_display_driver

 

+

AScha3_1-1763489780681.png

 

If you feel a post has answered your question, please click on " Best Answer ".
Associate
Nov 19, 2025 6:03 AM UTC

Dear Sir/Madam,

Thank you for your response. As requested, I am sharing the configuration details used in my STM32F401RE setup with the 3.5” SPI TFT Display (ILI9488). PIN CONFIGURATION

VCC - 3.3V , GND - GND , TFT_CS - PA4 (A2), TFT_DC - PA2 (D1), TFT_RST - PA1 (A1), TFT_SCK- PA5(D13)

, TFT_MOSI - PA7 (D11), TFT_MISO - PA46(D12), LED - 3.3V

BELOW I ADD SCREENSHOT OF MY IOC