Skip to main content
arnold_w
Senior II
Jan 29, 2024 1:01 PM UTC
Solved

Unable to connect to STM32F407-DISC1 with STM32 ST-LINK Utility and STM32CubeProgrammer

I'm unable to connect to STM32F407-DISC1. STM32 ST-LINK Utility gives "No ST-LINK detected" and STM32CubeProgrammer gives "Error: No debug probe detected". I run Windows 10 Business on a Lenovo ThinkPad P1 Gen 3 computer and I have tried with 2 different STM32F407-DISC1 boards, 2 different USB-cables and with both STM32 ST-LINK Utility versions 4.1.0 and 4.6.0. When I plug in my board, an additional "USB Composite Device" shows up under "Universal Serial Bus Controllers" in the Device Manager, but it won't let me manually update the driver to the one inside the en.stsw-link009-folder. I have tried to uninstall STM32 ST-LINK Utility, reboot my computer and install STM32 ST-LINK Utility again, but to no avail. Can someone please help me?

STLiink.jpg

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Jan 29, 2024 5:09 PM UTC

Do you get the Windows Ding-Dong sound when attaching?

Does the device show up in Device Manager? If not it's not going to be found by ST's tools.

Get the right driver loaded. Make sure to use a suitable cable. The charging cables with just power wired will not work, data wires needed.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

8 replies

mƎALLEm
ST Technical Moderator
Jan 29, 2024 1:45 PM UTC

Hello,

Could you try with another USB port on you PC? moreover try with another PC/Laptop

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
arnold_w
arnold_wAuthor
Senior II
Jan 29, 2024 2:56 PM UTC

I tried it on my colleague's laptop with STM32CubeProgrammer and got: "Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication"

mƎALLEm
ST Technical Moderator
Jan 29, 2024 3:44 PM UTC

Did you connect to these boards previously or it's the first time you're doing it?

Are you sure the boards are not broken?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
arnold_w
arnold_wAuthor
Senior II
Jan 29, 2024 4:05 PM UTC

Did you connect to these boards previously or it's the first time you're doing it? We used them many years ago

Are you sure the boards are not broken? But 2 boards with the same problem?

mƎALLEm
ST Technical Moderator
Jan 29, 2024 4:10 PM UTC

Ok but are they new? Are they yours originally? 

It could be broken and thrown by their original owner.. Who knows ..

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Jan 29, 2024 5:09 PM UTC

Do you get the Windows Ding-Dong sound when attaching?

Does the device show up in Device Manager? If not it's not going to be found by ST's tools.

Get the right driver loaded. Make sure to use a suitable cable. The charging cables with just power wired will not work, data wires needed.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..